ECAT.ENRXWARN
Description
ECAT.ENRXWARN allows enabling/disabling warning W7011, which is triggered when Rx data is received from the EtherCAT
***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs master before the drive finished preparing its TX data within a sync0 cycle.
-
- This warning will not be triggered when running at 250 μs cycle times as it is normal for the TX data to be from the prior cycle at this rate..
| Value | Description |
|---|---|
| 0 | W7011 cannot be triggered |
| 1 | W7011 can be triggered |
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-06-03-000 | - |
General Information
|
Type |
NV Parameter |
|
Units |
n/a |
|
Range |
0 to 1 |
|
Default Value |
1 |
|
Data Type |
Integer |
Variants Supported
Fieldbus
A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design variants: AKD2G-SPE